Metallpriser

Metallråvarupriserna tillhandahålls av InfoMine.com.

Den information om metallpriser som visas här finns för närvarande endast tillgänglig på engelska.

Välj de alternativ som du önskar få information om och klicka på "Display Chart".

Commodity: Per:
 
Currency:
Period:  
 



The prices of metals in the currencies of countries that mine the commodities can vary considerably from prices commonly quoted in the press, most of which are denominated in US dollars. Ultimately, it's the price of the metal in the domestic currency that's of importance to the metal miner. As such, the dollar exchange rate is a crucial aspect in determining the profitability of a mining company that sells a product internationally.

 

SRK Sweden